FB#.SCALED.PIN
Description
FB#.SCALED.PIN is the numerator of the FB#.SCALED.P scaling ratio.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-01-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 4,294,967,295 |
|
Default Value |
360 |
|
Data Type |
Integer |
|
See Also |
|
| Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.